:REPository:DUT:SERial
Meas. mode:
Scope
Eye
Jitter
TDR
Publish mode:
Selected
Custom
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:DUT:SERial <DUT_serial_number>
Where <DUT_serial_number>
is a string. For example, "US00123456".
Query Syntax
:REPository:DUT:SERial?
Query Response
<string>
Description
Labels the published data as being measured from a Device Under Test (DUT) with a specific serial numbere. In the N8844A, this label is a property on which you can filter your data. For example, if you publish multiple Fall Time measurements from five different DUTs, you can view a scatter plot that groups the measurements according to the DUT serial numbers. The default value is "unspecified".
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.