:SOURce:DRATe
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :SOURce:SRATe command.
Command Syntax
:SOURceN:DRATe <rate>
<rate> is a double.
Where N identifies a simulated module's specific channel and must be selected from {1:8}{A|B|C|D}. For example, SOURce3C.
Query Syntax
:SOURceN:DRATe?
Description
On simulated modules, sets the data rate for the specified source waveform. The data rate can be any value between 50 Mb/s and 160 Gb/s. Each waveform can be set to a different data rate. Click here for a list of standard optical and digital telecommunications rates.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
:SOURce:DRATe 8.5E+9