Reference Rx Operator
This Python example runs on PC and controls an N1010A FlexDCA application. The script installs a Reference Rx operator and, in Eye mode, returns TDECQ measurement. The script demonstrates the addressing of commands to the correct waveform function numbers.
Example Script
Copy
Reference-Rx-operator.py
""" Script on PC controls N1010A FlexDCA application. The script installs
a Reference Rx operator and, in Eye mode, returns TDECQ measurement.
Demonstrates the addressing of commands to the correct waveform function numbers.
"""
import pyvisa as visa # import VISA library
visa_address = 'TCPIP0::localhost::hislip0,4880::INSTR'
def open_flexdca_connection(address):
""" Opens visa connection to FlexFlexDCA. """
print('Connecting to Flexdca ...')
try:
rm = visa.ResourceManager()
connection = rm.open_resource(address)
connection.timeout = 10000 # Set connection timeout to 10s
connection.read_termination = '\n'
connection.write_termination = '\n'
inst_id = connection.query('*IDN?')
print('\nFlexDCA connection established to:\n' + inst_id, flush=True)
connection.query(':SYSTem:DEFault;*OPC?')
except (visa.VisaIOError, visa.InvalidSession):
print('\nVISA ERROR: Cannot open instrument address.\n', flush=True)
return None
except Exception as other:
print('\nVISA ERROR: Cannot connect to instrument:', other, flush=True)
print('\n')
return None
return connection
def all_channels_off(FlexDCA):
""" Turns all available channels off. """
for slot in '12345678':
for letter in 'ABCD':
channel = slot + letter
FlexDCA.write(':CHANnel' + channel + ':DISPlay OFF')
def install_simulated_module(FlexDCA):
""" Install a dual-optical simulated FlexDCA module. """
FlexDCA.write(':EMODules:SLOT1:SELection DOMini')
all_channels_off(flexdca)
FlexDCA.write(':SOURce1A:FORMat PAM4')
FlexDCA.write(':SOURce1A:WTYPe DATA')
FlexDCA.write(':SOURce1A:PATTern EPRBs15')
FlexDCA.write(':SOURce1A:SRATe 2.890000000E+10')
FlexDCA.write(':SOURce1A:AMPLitude 20E-3')
FlexDCA.write(':SOURce1A:NOISe:RN 2.50E-7')
FlexDCA.write(':SOURce1A:JITTer:RJ 1.0E-12')
FlexDCA.write(':CHANnel1A:DISPlay ON')
FlexDCA.write(':ACQuire:RUN')
FlexDCA.query(':SYSTem:MODE EYE;*OPC?')
FlexDCA.query(':TRIGger:PLOCk ON;*OPC?')
FlexDCA.query(':SYSTem:AUToscale;*OPC?')
def install_Ref_Rx_operator(FlexDCA):
""" Installs Reference Rx operator and CTLE secondary operator. Displays the waveforms.
TDECQ and DFE equalizers are installed by default.
:SPRocess commands addressed to Reference Rx (F1)
:FUNCtion commands addressed to CTLE (F2), TDECQ (F3), DFE (F4)
"""
FlexDCA.write(':FUNCtion1:FOPerator RRX')
FlexDCA.write(':SPRocess1:RRX:SIFunctions ON') # show secondary operators
FlexDCA.write(':FUNCtion1:SOP2 CTLequalizer') # install secondary CTLE equalizer
FlexDCA.write(':FUNCtion1:COLor TCOLor3') # Display Function 1 (Ref Rx waveform)
FlexDCA.write(':FUNCtion1:DISPlay ON')
FlexDCA.write(':FUNCtion2:COLor TCOLor4') # Display Function 2 (CTLE waveform)
FlexDCA.write(':FUNCtion2:DISPlay ON')
FlexDCA.write(':FUNCtion3:COLor TCOLor6') # Display Function 3 (TDECQ waveform)
FlexDCA.write(':FUNCtion3:DISPlay ON')
FlexDCA.write(':FUNCtion4:COLor TCOLor7') # Display Function 4 (DFE waveform)
FlexDCA.write(':FUNCtion4:DISPlay ON')
FlexDCA.write(':DISPlay:WINDow:TIME1:DMODe STILed')
def config_Ref_Rx(FlexDCA):
""" :SPRocess commands addressed to Reference Rx (F1) """
FlexDCA.write(':SPRocess1:RRX:PROPtimize ON')
FlexDCA.write(':SPRocess1:RRX:RPOint ASOP2')
def config_Secondary_CTLE(FlexDCA):
""" :SPRocess commands addressed to Reference Rx (F1)
:FUNCtion commands addressed to CTLE (F2)
"""
FlexDCA.write(':SPRocess1:CTLequalizer:ZERo1 4.200E+9')
FlexDCA.write(':FUNCtion2:VTRacking MANual')
FlexDCA.write(':FUNCtion2:YSCale 4.5E-3')
def config_Secondary_TDECQ(FlexDCA):
""" :SPRocess commands addressed to Reference Rx (F1) """
FlexDCA.write(':SPRocess1:TEQualizer:FIBer:ENABle ON')
FlexDCA.write(':SPRocess1:TEQualizer:FIBer:BANDwidth 2.96E+10')
FlexDCA.write(':MEASure:TDEQ:TSER 4.50E-4')
def config_Secondary_DFE(FlexDCA):
""" :SPRocess commands addressed to Reference Rx (F1) """
FlexDCA.write(':SPRocess1:DFEQualizer:PROPtimize:LTMagnitudes ON')
FlexDCA.write(':SPRocess1:DFEQualizer:PROPtimize:BMAX 4.1E-1, 3.5E-1, 1.2E-1, 1.0E-1')
FlexDCA.write(':SPRocess1:DFEQualizer:TAPS:AUTo OFF')
FlexDCA.write(':SPRocess1:DFEQualizer:PROPtimize:TAPS 2.7043E-2, 7.5E-5, -1.8686E-2, -9.465E-3')
def measure_tdecq(FlexDCA):
""" Returns a scalar TDECQ measurement result. """
import time
class ScalarMeasQuestionableException(Exception):
""" A scalar measurement result is questionable. """
pass
class ScalarMeasTimeOutException(Exception):
""" A scalar measurement has timed out. """
pass
timeout = FlexDCA.timeout / 1000 # convert ms to s
start_time = time.time() # time in seconds
flexdca.write(':MEAS:EYE:TDEQ')
while(True):
time.sleep(0.2)
status = FlexDCA.query(':MEAS:EYE:TDEQ:STATus?')
if 'CORR' in status: # valid measurement result
return FlexDCA.query(':MEAS:EYE:TDEQ?') # get measurement
elif 'QUES' in status: # questionable results
s = ':MEAS:EYE:TDEQ\nReason: ' + FlexDCA.query(':MEAS:EYE:TDEQ:STATus:REASon?')
raise ScalarMeasQuestionableException(s)
elif (int(time.time() - start_time)) > timeout: # IO timout
s = ':MEAS:EYE:TDEQ\nReason: ' + FlexDCA.query(':MEAS:EYE:TDEQ:STATus:REASon?')
raise ScalarMeasTimeOutException(s)
flexdca = open_flexdca_connection(visa_address)
install_simulated_module(flexdca)
install_Ref_Rx_operator(flexdca)
config_Ref_Rx(flexdca)
config_Secondary_CTLE(flexdca)
config_Secondary_TDECQ(flexdca)
config_Secondary_DFE(flexdca)
flexdca.write(':SPRocess1:RRX:RECalculate')
tdecq = measure_tdecq(flexdca)
print('TDECQ measures: ' + tdecq + ' dB')
flexdca.write(':SYSTem:GTLocal')
flexdca.close()