Measurement Flowchart
Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
This flowchart includes measurement blocks for jitter analysis, PJ frequency analysis, and interference analysis. If one of these measurements is turned off or unavailable, the block in the flowchart is simply skipped. Each time that the RJ and PJ data is collected, a new rising edge and a new falling edge is targeted. Edges are targeted sequentially throughout the pattern. Each time that the RN and PI data is collected, a new logical 1 and a logical 0 is targeted. Bits are targeted sequentially throughout the pattern.