Difference Operator
The Difference operator processes each point in the input waveform such that the output is equal to x(n) ā x(nā1).
The operator's Display Setup configures the manner in which the resulting waveform is displayed including both vertical and horizontal scaling. For more information, refer to Common Display Settings.
The Difference operator is designed for a single-valued waveform, as opposed to an eye diagram. Be sure that your trigger setup results in a single-valued waveform at the input to this operator. This can be achieved using an external pattern trigger or by using pattern lock. If you are using an external pattern trigger, you may ignore this note.
The Difference operator is not available in Jitter mode.