Chord Signaling operators

Instrument
DCA-X
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye

The following Chord Signaling operators are available for use with newer encoding formats. An operator's output is automatically assigned to an output function. The function's waveform is not displayed unless you drag a function color icon onto the function's output. After placing chord operator, click on it to setup any available settings.