Jitter & Noise Settings
Instrument
N1000A
N1010A
Use the Configure Jitter & Noise dialog to add random jitter, random noise, and F/2 (Pk-Pk) jitter to a simulated waveform. If the simulated waveform is defined to be electrical differential, the amount of applied Resultant Differential RJ and Resultant Differential RN is listed. When applying F/2 (Pk-Pk) jitter, select an even pattern length for the simulated signal. For example, select PRBS-7 (128 UIs). Otherwise, the F/2 jitter measurement will not work.
The ability to add periodic jitter and interference was deleted starting with firmware revision A.02.00.