:CALibrate:MODule:PTIMebase:STATus:DETails?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Instruments:
N1093A/B-PTB
Query Syntax
:CALibrate:MODule:PTIMebase:STATus:DETails? "<DCA-M-module-name>"
Where <DCA-M-module-name> is the name that identifies an N1093A/B module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1093B-US12345678".
Description
Queries a string of status details of an N1093A/B DCA-M module's precision timebase calibration.
Requires FlexOTO revision A.07.90 and above.
Example Returned Status Strings
A typical returned string:
Time of last Calibration: 10/23/2012 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"
If a calibration is recommended:
"Elapsed cal time has exceeded 10 hours.,Time of last Calibration: 10/08/2012 11:13:37,Elapsed Calibration Time: 9 days,Temperature Change: -4.32 C"
If a calibration has not yet been performed:
"This calibration has never been performed in this instrument."