:CALibrate:MODule:PTIMebase:STATus:TIME?

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Instruments:
N1093A/B-PTB

Query Syntax

:CALibrate:MODule:PTIMebase:STATus:TIME? "<DCA-M-module-name>"

Where <DCA-M-module-name> is the name that identifies an N1093A/B module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1093B-US12345678".

Description

Queries the date and time of an N1093A/B DCA-M's last precision timebase calibration. If a calibration has not yet been performed, an empty string is returned.

Requires FlexOTO revision A.07.90 and above.

Example Returned Status String

"10/08/2012 11:13:37"