:CALibrate:MODule:PTIMebase
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Instruments:
N1093A/B-PTB
Command Syntax
:CALibrate:MODule:PTIMebase {ENABled | DISabled | PARTial} "<DCA-M-module-name>"
Where <DCA-M-module-name> is the name that identifies an N1093A/B DCA-M module on the Hardware Diagram. For example, "N1093B-US12345678".
Query Syntax
:CALibrate:MODule:PTIMebase? "<DCA-M-module-name>"
Query Response
{ENAB | DIS | PART}
Description
Enables or disables the precision timebase calibration on N1093A/B module.
- ENABled
-
Selects all precision timebase calibrations for the module to be performed. - DISabled
-
Prevents all precision timebase calibrations for the module from being performed. - PARTial
-
Indicates that some precision timebase calibrations are enabled and some are disabled.
To start the calibration, use the :CALibrate:MODule:STARt command.
Use the child queries listed in the following table to return details about the current calibration.
| Status String | Child Query to Send |
|---|---|
| State of Calibration | :STATus?
|
| Time of last calibration, Time change since last calibration, and Temperature change since last calibration |
:STATus:DETails?
|
| Change in temperature | :STATus:DTEMperature?
|
| Change in Time | :STATus:TIME?
|
Requires FlexOTO revision A.07.90 and above.