:CALibrate:MODule:PTIMebase:STATus:DTEMperature?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Instruments:
N1093A/B-PTB
Query Syntax
:CALibrate:MODule:PTIMebase:STATus:DTEMperature? "<DCA-M-module-name>"
Where <DCA-M-module-name> is the name that identifies an N1093A/B module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1093B-US12345678".
Description
Queries the change in an N1093A/B DCA-M's temperature from the time when the last precision timebase calibration was performed. If a calibration has not yet been performed, a value of NaA (9.91E+37) is returned. A calibration should be performed if the change in DCA-M's temperature exceeds ±5°C.
Example Returned Status
3.590000000E+00
Requires FlexOTO revision A.07.90 and above.