:CALibrate:MODule:UTIMebase:STATus?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Instruments:
N1093A/B
Query Syntax
:CALibrate:MODule:UTIMebase:STATus? "<DCA-M-module-name>"
Where <DCA-M-module-name> is the name that identifies an N1093A/B DCA-M module on the Hardware Diagram. For example, "N1093B-US12345678".
Query Response
{CALIBRATED | UNCALIBRATED}
Description
Returns the status of the timebase calibration for an N1093A/B module. Use the :CALibrate:MODule:UTIMebase:DETails, :CALibrate:MODule:UTIMebase:DTEMperature, and :CALibrate:MODule:UTIMebase:TIME child commands to return detailed information about the calibration status. Use the :CALibrate:MODule:UTIMebase command to include the user timebase calibration in a module calibration.
Requires FlexOTO revision A.07.90 and above.