:CALibrate:MODule:UTIMebase:STATus:DETails?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Instruments:
N1093A/B
Query Syntax
:CALibrate:MODule:UTIMebase:STATus:DETails? "<DCA-M-module-name>"
Where <DCA-M-module-name> is the name that identifies an N1093A/B DCA-M module on the Hardware Diagram. For example, "N1093B-US12345678".
Description
Returns a string that provides the date of the last timebase calibration for the indicated module as well as the elapsed time and the temperature (Celsius) change. Use the :CALibrate:MODule:UTIMebase:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string:
"Time of last Calibration: 01/08/2014 07:07:12,Elapsed Calibration Time: 8 days,Temperature Change: 1.73 C"
Requires FlexOTO revision A.07.90 and above.