:CALibrate:MODule:UTIMebase:STATus:DTEMperature?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Instruments:
N1093A/B
Query Syntax
:CALibrate:MODule:UTIMebase:STATus:DTEMperature? "<DCA-M-module-name>"
Description
Returns a string that provides the change in temperature (Celsius) from the last N1093A/B module timebase calibration. Use the :CALibrate:MODule:UTIMebase:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string, which indicates that the temperature of the module has risen 1.73°C:
"1.730000000E+00"
Requires FlexOTO revision A.07.90 and above.