:CALibrate:MODule:UTIMebase:STATus:TIME?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Instruments:
N1093A/B
Query Syntax
:CALibrate:MODule:UTIMebase:STATus:TIME? "<DCA-M-module-name>"
Where <DCA-M-module-name> is the name that identifies an N1093A/B DCA-M module on the Hardware Diagram. For example, "N1093B-US12345678".
Description
Returns a string that provides the time that has elapsed since the last N1093A/B module timebase calibration. Use the :CALibrate:MODule:UTIMebase:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string:
"01/09/2014 06:20:09"
Requires FlexOTO revision A.07.90 and above.