:CONFigure:STATus:REASon?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:CONFigure:STATus:REASon?
Description
Returns a string that explains the reason for an invalid Hardware Diagram. If the setup is correct, a null string is returned. Use the :CONFigure:STATus? parent query to determine if the Hardware Diagram is valid.
The returned string is the same string as is displayed in the GUI just above the Hardware Diagram. For example,
"Ensure the setup has at least 1 DUT fixture, 1 switch module, and 1 DCA-M module."