:CONFigure:WAVelength:VALue:VSET?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:CONFigure:WAVelength:VALue:VSET?
Query Response
<wavelength>,<wavelength>,...
For example, "1.310E-6,1.550E-6"
Description
Returns a comma separated string of all wavelengths supported by FlexOTO's Analysis Engine
An N1092A/B DCA- M with option CDR (clock recovery) or an N1092D / N107xA DCA-M combination that FlexOTO uses to get data.. To set a wavelength, use the :CONFigure:WAVelength:VALue command. Then, if you want to know the argument token associated with the :CONFigure:WAVelength command, use the :CONFigure:WAVelength? query.