:CONFigure:WAVelength
Command Syntax
:CONFigure:WAVelength {WAVelength1 | WAVelength2 | ...}
Query Response
{WAV1 | WAV2 | ...}
Description
Selects the wavelength of the waveform being measured on the Analysis Engine
An N1092A/B DCA- M with option CDR (clock recovery) or an N1092D / N107xA DCA-M combination that FlexOTO uses to get data. using a wavelength token argument. To learn what wavelength is associated with the token, use the :CONFigure:WAVelength:VALue? query.
To select the wavelength by entering the actual wavelength in meters, for example 1310 nm or 1550 nm, use the :CONFigure:WAVelength:VALue command. If the entered wavelength is not supported by the hardware, FlexOTO selects the closest valid wavelength (returned with the query) and the associated token will be returned by the :CONFigure:WAVelength? query. To return a list of all available wavelengths in meters, use the :CONFigure:WAVelength:VALue:VSET? query.
To set the wavelength setting on optical switches that support this setting, use the :CONFigure:SWITch:WAVelength command.