:CONFigure:WAVelength:VALue
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CONFigure:WAVelength:VALue <wavelength>
Where <wavelength> is in meters.
Query Response
<wavelength>
Description
Sets the wavelength of the waveform being measured in meters. For example, 1310 nm or 1550 nm. If a wavelength is entered is not supported by the hardware, FlexOTO selects the closest valid wavelength (returned with the query form of this command) and the associated token will be returned by the :CONFigure:WAVelength? query. To return a list of all available wavelengths, use the :CONFigure:WAVelength:VALue:VSET? query.
To set the wavelength setting on optical switches that support it, use the :CONFigure:SWITch:WAVelength command.