*ESE (Event Status Enable)

Flex Apps:
FlexDCA
FlexRT
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations

Command Syntax

*ESE <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

*ESE?

Description

Enters a decimal-weighted value into the Standard Status Enable Register. These bits mask the ability to report bits in the Standard Status Event Register.

Standard Status Register Commands
Register Read Write Command
Event ♦   *ESR?
Enable (mask) ♦ ♦ *ESE
Standard Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
PON URQ CME EXE DDE QYE RQL OPC
Enable
Register
               
Sets to Bit 5 (ESB) in Status Byte Register

Bit Definitions

OPC
A true indicates that an operation is complete.
RQL
Not used. Permanently set to zero.
QYE
A true indicates that a query error has been detected.
DDE
A true indicates that a device-dependent error has been detected.
EXE
A true indicates that an an execution error has been detected.
CME
A true indicates that a command error has been detected.
URQ
Not used. Permanently set to zero.
PON
A true indicates that an off-to-on transition has occurred.