*IDN? (Identification Number)
Flex Apps:
FlexDCA
FlexRT
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Query Syntax
*IDN?
Query Response
"Keysight Technologies,<model-number>,<computer-name>,<application-version>"
Description
Returns an ASCII string that lists FlexOTO application model number, the PC's computer name where FlexPLL is installed, and FlexOTO's firmware version. This is shown in the following example,
"Keysight Technologies,N1000100A,CQR8329,A.06.60.23"
The model numbers that are returned for the various Flex applications are listed in the following table.
| Application | Model Number |
|---|---|
| FlexDCA (on N1000A) | N1000A |
| FlexDCA (on PC) | N1010A |
| FlexPLL | N1000100A |
| FlexOTO (Hardware Diagram) | N1000300A |
| FlexOTO (Station) | N1000200A |