*TRG (Trigger)
Flex Apps:
FlexDCA
FlexRT
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
*TRG
Description
Acquires data for the test plan, if the test plan conditions are met. The *TRG common command has the same effect as the :TPRogram:RUN? command with the exception that the command does not return a comma delimited string of integers representing job IDs.