:DISK:SIMage:FNAMe:AUPDate
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:DISK:SIMage:FNAMe:AUPDate
Description
Increments a file name's autonumber for the next file saved with the :DISK:SIMage:SAVE command. The autonumber is placed at the end of the file name and begins with a hyphen followed by decimal digits:
<type_><YYYY-MM-DD><_autonumber>.<extension>
An example autonumber would be Screen_2020-10-23_1.jpg. Saving a file with :DISK:SIMage:SAVE does not increment the autonumber. You must use the :DISK:SIMage:FNAMe:AUPDate command to increment the autonumber. Otherwise, the next file saved will have the same name as the last file saved.
If you have entered a custom file name, but want to return to using standard file name, use the :DISK:SIMage:FNAMe:USTandard command.
| Name | Type | Autonumber | Default Extension |
|---|---|---|---|
| Screen_2017-04-08_1 | standard | yes | .jpg |
| DUT | custom | no | .jpg |
| DUT23 | custom | no | .jpg |
| DUT_23 | custom | yes | .jpg |
Example Command Sequence
:DISK:SIMage:FNAMe "my_file_1.png" :DISK:SIMage:SAVE # my_file_1.png … … :DISK:SIMage:FNAMe:AUPDate :DISK:SIMage:SAVE # my_file_2.png