:DISK:SIMage:IMETadata
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:DISK:SIMage:IMETadata {ON | OFF}
Query Syntax
:DISK:SIMage:IMETadata?
Description
Turns on and off the inclusion of metadata when saving a screen image file using the :DISK:SIMage:SAVE command. Saving metadata only applies to screen captures that are saved as jpg or tiff file formats. To view or edit the metadata placed in your screen image file, you can right click on the file in Window's File Explorer and from the shortcut menu select Properties. In the Properties dialog, click the Details tab. To edit the metadata fields for your image, click on the Value entree shown on the dialog. The following table lists the metadata fields that FlexOTO populates. The query form of the command returns the current setting.
| Metadata Field | Value Examples |
|---|---|
| Subject | Screen Capture |
| Comments | N1000A (S/N USXXXXXXXX) Modules: Slot 1 Module (MYXXXXXXXX) |
| Date taken | 10/23/2020 4:32 PM |
| Program name | FlexOTO (A.0X.XX.XXX) |
| Camera maker | Keysight Technologies |
| Camera model | FlexOTO (A.0X.XX.XXX) |
| Name | ScreenCapture.jpg |