:DISK:SIMage:FNAMe:USTandard
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:DISK:SIMage:FNAMe:USTandard
Description
Resets the file name for the screen image file from using a custom name to using the standard name in the following form:
Screen_<date><autonumber>.<extension>
For example, Screen_2020-10-23_1.jpg. Refer to :DISK:SIMage:FNAMe to learn about standard and custom names.