:JOBS:RESults:MEASure:CEQ:STATus:REASon?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:RESults:MEASure:CEQ:STATus:REASon? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
"<reason>"
For example, "No Data". Notice that the response includes double quotes.
Refer to the table "Possible Common :STATus:REASon? Query Responses".
Description
For the specified Job ID, queries a string that explains the reason for a failed :JOBS:RESults:MEASure:CEQ measurement. If the measurement was successful, a null string is returned.
Additional information about the failure may be available using the :JOBS:RESults:MEASure:CEQ:STATus:DETails? sibling query. Use the :JOBS:RESults:MEASure:CEQ:STATus? parent query to determine if the measurement has failed.