:CALibrate:MODule:CRECovery:STATus?
Flex Apps:
FlexPLL
FlexOTO
Query Syntax
:CALibrate:MODule:CRECovery:STATus?
Description
Queries the status of the JTF Receiver module's clock recovery. One of the following response strings is returned:
- "CALIBRATED"
- The clock recovery capability does not require a calibration.
- "UNCALIBRATED"
- The module capability requires a calibration.
Use the following child queries to return details about the current calibration.
| Status String | Query to Send |
|---|---|
| CALIBRATED or UNCALIBRATED |
:CALibrate:MODule:STATus?
:CALibrate:MODule:CRECovery:STATus?
|
| Time of last calibration, time change since last calibration, and temperature change since last calibration |
:CALibrate:MODule:STATus:DETails?
:CALibrate:MODule:CRECovery:STATus:DETails?
|
| Change in temperature | :CALibrate:MODule:STATus:DTEMperature?
:CALibrate:MODule:CRECovery:STATus:DTEMperature?
|
| Change in Time | :CALibrate:MODule:STATus:TIME?
:CALibrate:MODule:CRECovery:STATus:TIME?
|
Requires FlexDCA revision A.06.60 and above for FlexPLL.