:CALibrate:MODule:CRECovery:STATus:DETails?
Flex Apps:
FlexPLL
FlexOTO
Query Syntax
:CALibrate:MODule:CRECovery:STATus:DETails?
Description
Queries a string of status details of the JTF Receiver module's clock recovery calibration. The following is an example of a typical returned string:
Time of last Calibration: 10/23/2024 11:52:00, Elapsed Calibration Time: 3 hours 2 minutes, Temperature Change: 1.24 C"
If a calibration is recommended, the following text is placed at the beginning of the above string:
"Requires Clock Recovery Calibration, …"
If a calibration has not yet been performed, the following string is returned:
"This calibration has never been performed in this instrument."
Example Returned Status String
"Elapsed cal time has exceeded 10 hours.,Time of last Calibration: 09/20/2012 15:11:05, Elapsed Calibration Time: 26 days,Temperature Change: 2.58 C"
Requires FlexDCA revision A.06.60 and above for FlexPLL.