:CALibrate:MODule:ENABled
Flex Apps:
FlexPLL
Command Syntax
:CALibrate:MODule{1:8}:ENABled {ENABled | DISabled}
Query Syntax
:CALibrate:MODule:ENABled?
Query Response
{ENAB | DIS}
Description
For the specified DCA-M module, enables or disables a vertical and clock-recovery calibration for the indicated module.
- ENABled
- Selects all calibrations for the module to be performed.
- DISabled
- Prevents all calibrations for the module from being performed.
Use the following child queries to return details about the current calibration.
| Status String | Query to Send |
|---|---|
| CALIBRATED or UNCALIBRATED |
:CALibrate:MODule:STATus?
:CALibrate:MODule:CRECovery:STATus?
|
| Time of last calibration, time change since last calibration, and temperature change since last calibration |
:CALibrate:MODule:STATus:DETails?
:CALibrate:MODule:CRECovery:STATus:DETails?
|
| Change in temperature | :CALibrate:MODule:STATus:DTEMperature?
:CALibrate:MODule:CRECovery:STATus:DTEMperature?
|
| Change in Time | :CALibrate:MODule:STATus:TIME?
:CALibrate:MODule:CRECovery:STATus:TIME?
|
Requires FlexPLL revision A.06.70 and above.