:CALibrate:MODule:STATus:DTEMperature?

Flex Apps:
FlexPLL
FlexOTO

Query Syntax

:CALibrate:MODule:STATus:DTEMperature?

Description

Queries the change in the JTF Receiver module's channel temperature (°C) from the time when the last channel calibration was performed on the indicated channel. If a calibration has not yet been performed, a value of NaA (9.91E+37) is returned. A calibration should be performed if the change in DCA-X temperature exceeds ±5°C.

Example Returned Status

2.340000000E+00

Requires FlexPLL revision A.06.70 and above.