:CALibrate:MODule:CRECovery:STATus:TIME?

Flex Apps:
FlexPLL
FlexOTO

Query Syntax

:CALibrate:MODule:CRECovery:STATus:TIME?

Description

Queries the date and time when the JTF Receiver module's last clock recovery calibration was performed. If a calibration has not yet been performed, an empty string is returned.

Example Returned Status String

"09/20/2012 15:11:05"

Requires FlexDCA revision A.06.60 and above for FlexPLL.