:RDCA:CONNect:GPIB:ADDRess
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:RDCA:CONNect:GPIB:ADDRess <address>
<address> is an integer.
Query Syntax
:RDCA:CONNect:GPIB:ADDRess?
Description
Enters a N1000A's GPIB address for connecting via GPIB. Use the :RDCA:CONNect:METHod command to specify a GPIB connection. The address can be any integer from 0 to 30. The default value is 7. To locate the N1000A's GPIB address, click Tools > Remote Interface on the N1000A's menu. Use the :RDCA:CONNect:GPIB:INAMe command to specify the GPIB interface's name.
Example Command Sequence
:RDCA:CONNect:METHod GPIB :RDCA:CONNect:GPIB:ADDRess 7 :RDCA:CONNect:GPIB:INAMe "gpib3" :RDCA:CONNect