:RDCA:CONNect:HOST
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:RDCA:CONNect:HOST "hostname"
Where "hostname" is a string that is the Computer Name in FlexDCA's About dialog. This command supports the DEFault common child command.
Description
Sets or queries the current host name of a N1000A when connecting to the instrument via a LAN. Use the :RDCA:CONNect:METHod command to specify a LAN connection. Use the :RDCA:CONNect command to make the actual connection.