:RDCA:CONNect:STATe?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:RDCA:CONNEct:STATe?
Description
Queries the state of the connection between FlexPLL and an N1000A. Returns one of the following strings:
CONN- A flex-on-flex connection is established to an N1000A.
NCON- A connection is not established.
TOUT- A flex-on-flex connection to an N1000A has timed out.
- To combine with other queries to determine FlexDCA's configuration.