:RDCA:CONNect:HLAN:PORT
Flex Apps:
FlexPLL
Command Syntax
:RDCA:CONNect:HLAN:PORT <port number>
<port number> is an integer.
Query Syntax
:RDCA:CONNect:HLAN:PORT?
Description
Use this command with FlexPLL to enter a HLAN Port number for a N1000A for connecting via the HLAN LAN protocol. The port number default value is 4880. Use the :RDCA:CONNect:HLAN:INDEX command to specify Device Index for the connection. Use the :RDCA:CONNect:METHod command to specify a LAN connection. Use the :RDCA:CONNect:LSERver command to specify the type of LAN server: HLAN.