:RDCA:CONNect:LSERver
Flex Apps:
FlexPLL
Command Syntax
:RDCA:CONNect:LSERver {HLAN | VLAN}
Query Syntax
:RDCA:CONNect:LSERver?
Description
Use this command with FlexPLL when connecting FlexPLL to an DCA-X JTF receiver via LAN, you can selects the type of LAN server used to make the connection. The following three protocols are available:
- VLAN (default setting)
- Selects a Virtual Local Area Network (VLAN). This is the VXI-11 selection for LAN Server in FlexPLL's Receiver Setup dialog. Use this command to configure the server:
- HLAN
- Selects a High Speed Local Area Network (HLAN). This is the HiSLIP selection for LAN Server in FlexPLL's Receiver Setup dialog. Use these commands to configure the server: