:RDCA:CONNect:VLAN:INDEX
Flex Apps:
FlexPLL
Command Syntax
:RDCA:CONNect:HLAN:INDEX <device index>
<device index> is an integer.
Query Syntax
:RDCA:CONNect:HLAN:INDEX?
Description
Use this command with FlexPLL to enter a VLAN Device Index for the DCA-X for connecting via the VLAN LAN protocol. The Device Index can be any integer from 0 to 30. The default value is 0. Use the :RDCA:CONNect:METHod command to specify a LAN connection. Use the :RDCA:CONNect:LSERver command to specify the type of LAN server: HLAN or VLAN.