Pulse Table (Advanced-Radar/Hopping)
Menu Path:
This trace is only available when the Synchronization Domain is Amplitude or the Pulsed checkbox is checked. If both of these are not true, the trace won't be available for selection.
The Pulse Table is a type of Matrix Table that includes all pulse-specific result metrics, measured over all valid, synchronized, pulse-analysis time samples detected within the time specified by Acquisition Length.
All displayed metrics in the table (except for Pulse index) are measured over the pulse-specific, synchronized, user-specified analysis time samples as determined by the Detection settings.
When averaging is turned on, the reported metrics are averaged.
You can highlight one row, then right-click and select Set Start Pulse to conveniently set the Starting Pulse.
Sorting by metric
You can sort the table by any metric by left-clicking the metric name. Click again to toggle between ascending or descending order. Cancel sorting by right-clicking and selecting "Clear Sort".
See Also