Waveform Generation Parameters (Flex Frame - Basic and Advanced Modes)

The Waveform Generation parameter group configures the settings needed to define the generated Flex Frame signal, predistort the waveform with the measured EQ response, add AWGN Additive White Gaussian Noise - Statistically random radio noise characterized by a wide frequency range with regards to a signal in a communications channel. and recall as a recording, save to a file or download to a source.

Signal Length – Specifies the signal length. When Auto is enabled, if the signal is periodic, the waveform length is the frame length. If the signal is burst but length is variable length, the waveform length will be the result length. If the signal is burst with fixed length, the waveform length is the frame length.

Default: 1000 Symbols, Auto = Enabled (selected)

Idle(Pre) Length – Specifies the pre-idle length. Idle(Pre) Length is only applied when Frame Type is Burst (Advanced mode) or Pulse Search is checked (Basic mode). It is not applied to Periodic waveforms.

When Idle(Pre) Length Auto is enabled, if the signal is periodic, the length is 0. If the signal is burst, the length in seconds will be Search Length in seconds / 2.2 - signal length in seconds to make sure that the current search length contains at least 2 burst. If this value is negative, the current search length is too short for current burst and the Idle(Pre) Length will be set to 1000 to make sure the final signal is still burst. You may need to make the search length longer (> 2.2 * waveformLength) to ensure a good burst and the measurement is stable.

Default: 500 Symbols, Auto = Enabled (selected)

Idle(Post) Length – Specifies the post-idle length. Idle(Post) Length is only applied when Frame Type is Burst (Advanced mode) or Pulse Search is checked (Basic mode). It is not applied to Periodic waveforms.

When Idle(Post) Length Auto is enabled, if the signal is periodic, the length is 0. If the signal is burst, the length in seconds will be Search Length in seconds / 2.2 - signal length in seconds to make sure that the current search length contains at least 2 burst. If this value is negative, the current search length is too short for current burst and the Idle(Post) Length will be set to 1000 to make sure the final signal is still burst. You may need to make the search length longer (> 2.2 * waveformLength) to ensure a good burst and the measurement is stable.

Default: 500 Symbols, Auto = Enabled (selected)

Oversample Ratio – Specifies the oversample ratio of the waveform.

Default: 4

Predistortion – Applies linear channel unflatness pre-compensation (FIR Finite Impulse Response filter) to the waveform based on the measured EQ response calculated in the Eq Correction Spectrum trace.

Default: Off

Choices: Off, Measured Channel

AWGN

AWGN Added – Enables or disables adding AWGN to the generated Flex Frame waveform.

Default: Disabled (cleared)

Carrier To Noise Ratio – For bursted signals, when AWGN is enabled for the waveform with the specified Carrier To Noise Ratio, the noise is added over the whole signal (active and inactive part), but the Carrier To Noise Ratio is the ratio of the active signal power over the noise power.

Default: 40 dB

IQ Impairments

IQ Impairments – determines IQ impairments are applied to the waveform.

Default: Off

Choices: Off, User Defined, Measured IQ Impairments

I Offset(%) – (IQ Impairments = User Defined) defines the I offset as a percentage relative to the magnitude of the I channel.

Default: 0

Q Offset(%) – (IQ Impairments = User Defined) defines the Q offset as a percentage relative to the magnitude of the Q channel.

Default: 0

IQ Gain Imbalance(dB) – (IQ Impairments = User Defined) defines the gain difference (in dB) between Q and I channels. Positive values mean Q has more power than I.

Default: 0

IQ Quad Imbalance(deg) – (IQ Impairments = User Defined) additional phase offset on the Q path. Positive values mean Q phase is advanced.

Default: 0

IQ Time Skew(s) – (IQ Impairments = User Defined) defines the time delay (in seconds) applied to the Q path relative to I. Positive values mean Q is delayed.

Default: 0

Range: ± symbol duration

Read-only information about the waveform

Advanced configuration mode Basic configuration mode

Recall As Recording – Recalls the currently configured Flex Frame signal as a recording using the Waveform Generation settings. Recall As Recording automatically recalls the current waveform as a recording and begins to play it. For configurations with multiple component carriers (Advanced configuration mode), the waveform with the selected Component Carrier is recalled. If Component Carrier is set to All, only the first CC's waveform is recalled.

Download to Source – Downloads a waveform created based on the current Flex Frame configuration to a properly configured, connected source. For configurations with multiple component carriers (Advanced configuration mode), the waveform with the selected Component Carrier is downloaded. If Component Carrier is set to All, only the first CC's waveform is downloaded.

Save to File – Saves the currently configured Flex Frame signal as one or more VSA MATLAB (.mat) waveform files, depending on the number of component carriers and the Component Carrier selection. For configurations with multiple component carriers (Advanced configuration mode), if Component Carrier is set to All, when you click Save to File, a file is generated for each CC.

 

•

See Also

Waveform Generation Tab

Flex Frame Properties Dialog Box