About Analog Input Properties (Acquisition)

Menu Path: Acquisition > Amplitude

The Analog Input Properties specify the range, coupling and input impedance of the input measurement hardware. The Analog Input Properties are located on the Analog tab of the Input dialog box (Acquisition > Amplitude). Some properties may be unavailable depending upon the number or type of Input Channels specified for the current measurement.

The input measurement hardware is configured in the Configurations tab of the Hardware dialog box. The input measurement hardware to use for the current measurement is specified in the Current Analyzer Configuration parameter and can also be specified by the Hardware Analyzer menu (Hardware > Analyzer).

The Analog tab provides the following:

Some of the parameters may be unavailable depending upon the number or type of channels available and the channels selected for the current measurement.

See Also

About Input Channels

About Hardware

Configurations Tab (Hardware)