Window Menu

The Window menu provides these selections to open specific VSA windows and configure trace layout:

This menu item…

Does this…

 

 

Output / Show .NET or SCPI

Opens the Output Window to view output from macros as well as the corresponding .NET API 1) Access Preamble Indicator, or 2) Application Programming Interface code if a VSA setting is changed.

 

 

SCPI Log

Opens the SCPI Log Window at the bottom of the trace window, which allows you to view SCPI commands sent to/from the VSA.

 

 

Event Log

Opens the Event Log Window to view events that occur when running Event Based Actions.

 

 

Contexts

Opens the Contexts Window which contains controls for managing contexts.

 

 

Block Diagram

Opens the Block Diagram Window, which is a left- to right-flowing visual representation of the VSA measurement setup.

 

 

Macros

Opens the Macros Window which contains buttons that run the macros loaded in the Macros dialog.

 

 

Trace Layout

Provides multiple selections for configuring how trace windows are arranged in the main window.

 

 

New Trace Window

Creates an empty Trace Window.

 

 

Resize Traces

Evenly distributes the height and width of all trace windows docked in the main window.

 

 

Collect Traces

Moves all traces for a measurement into the current window.