Recalling Multiple Recordings
Recall Multiple Recording recalls multiple single-channel recordings at once, allowing you to configure multi-channel measurements in a single operation. The Recall Multiple Recordings feature can recall recordings saved in the .binf, .csv, .mat, .bin, .orb, .sdf/.dat, txt and .vita49 file formats.
The following conditions apply when recalling multiple recordings:
- The recording files must have the same values defined for Data Header keys such as:
- For files with different data lengths, the shortest length will be used as the recall length for all files.
Follow these steps to recall a recording (or simply drag and drop a recording over the VSA application window).
- Click .
- In Recall Multiple Recording dialog, browse and Shift-click or Ctrl-click to select the recordings to be used in the multi-channel measurement.
Each selected recording will be assigned a channel and displayed in the File Information Preview area of the dialog.
- Choose a Padding Selection and Padding Mode if desired.
- Click .
Select Input > Recording > Info to view a list of the currently recalled recording files.
You can also combine all of the recorded channels into a single file by selecting File > Save > Save Recording.
Recordings are saved in a temporary recording file which is overwritten when a new recording is created or a recording is recalled. To preserve the current recording, rename and save the temporary recording file before creating a new recording.
Open the recording Player (
), the player makes recording and playing back easier to control and manipulate.See Also