Modulation Analysis (802.15.4 HRP UWB)
determines whether the contents of the IQ Meas Time, IQ Ref Time, Err Vect Time, Decoded Bits and Demodulated Bits traces are available and whether NRMSE is computed. This setting is only available if Data Power Analysis is enabled.
You can improve measurement speed by disabling Modulation Analysis if you don't need these metrics.
Default: Enabled
See Also