Bit Pattern (RFID)
: Cleared (See RFID Standard Setups/Presets Table)
specifies the bit pattern used by the sync search. Enter the desired bit pattern in the text box labeled .
The radio button is enabled when is selected. It is disabled when is not selected.
sync search is not available when the standard is selected because the Raw Demod Bits trace is not available.
searches the trace for the pattern entered in the text box. If the operation finds the specified pattern, that pattern is highlighted in the Raw Demod Bits trace.
See Also