Sync Offset (RFID)

Default:  0 Sec (See RFID Standard Setups/Presets Table)

Sync Offset specifies, in seconds, the start of the demodulated data as an offset from the location of the sync pattern.

The Sync Offset text box becomes active when Analysis > RFID Demod Properties > Time tab > Burst Search Off is selected and Analysis > RFID Demod Properties > Sync Search tab > Sync Search is selected.  

See Also

Burst Search

Burst Index

Result Length

Result Offset

Sync Search Offset

Sync Search Tab (RFID Demod Properies)