Result Offset (RFID)
1 mSec (See RFID Standard Preset Table)
0 to ( - )
The parameter sets the measurement start time interval in relation to acquisition time.
The box becomes active when both is set to and is not selected. The box becomes inactive when either is set to or is selected.
Selecting disables the parameter because determines when the results should be measured.
The following diagram shows result-related parameters:
See Also
Sync Search Tab (RFID Demod Properties)