[:SENSe]:CORRection:ENR:SPOT:COVerage <char>

(Read-Write) Set and query the value of the ENR uncertainty coverage (1σ, 2σ, or 3σ).

Note: Only available when CORR:ENR:MOD is set to SPOT.

See also [:SENSe]:CORRection:ENR:MODe, [:SENSe]:CORRection:ENR:SPOT:ENR, [:SENSe]:CORRection:ENR:SPOT:UNCertainty, [:SENSe]:CORRection:ENR:SPOT:ONGamma, [:SENSe]:CORRection:ENR:SPOT:OFFGamma, [:SENSe]:CORRection:ENR:SPOT:SPECify, [:SENSe]:CORRection:ENR:SPOT:DISTribution, and [:SENSe]:CORRection:TCOLd.

Relevant Modes

 NF

Parameters

 

<character>

ENR Spot mode's ENR uncertainty coverage value. Choose from:

SD1 - 1σ (About 68% of the values fall within 1 standard deviation of the mean.)

SD2 - 2σ (About 95% of the values fall within 2 standard deviations of the mean.)

SD3 - 3σ (About 99.7% of the values fall within 3 standard deviations of the mean.)

Examples

CORR:ENR:SPOT:COV SD1

CORR:ENR:SPOT:COV SD3

Query Syntax

CORRection:ENR:SPOT:COV?

Return Type

Character

Default

SD2


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)