[:SENSe]:CORRection:ENR:SPOT:ONGamma <num>

(Read-Write) Set and query the On value (hot) of the ENR spot value’s 50Ω match, Γ (0.000 to 1.000).

Note: Only available when CORR:ENR:MOD is set to SPOT.

See also [:SENSe]:CORRection:ENR:MODe, [:SENSe]:CORRection:ENR:SPOT:ENR, [:SENSe]:CORRection:ENR:SPOT:UNCertainty, [:SENSe]:CORRection:ENR:SPOT:OFFGamma, [:SENSe]:CORRection:ENR:SPOT:COVerage, [:SENSe]:CORRection:ENR:SPOT:SPECify, [:SENSe]:CORRection:ENR:SPOT:DISTribution, and [:SENSe]:CORRection:TCOLd.

Relevant Modes

 NF

Parameters

 

<numeric>

ENR Spot mode's 50Ω match, Γ On value (hot). Choose from:

Minimum of 0.000 up to

Maximum of 1

Examples

CORR:ENR:SPOT:ONG .2

CORR:ENR:SPOT:ONG 0.347

Query Syntax

CORRection:ENR:SPOT:ONGamma?

Return Type

Numeric

Default

0.000E+00


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)