(Read-Write) Set and query the ENR specified fixed value. This value indicates the nature of the entered value relative to the population of values it represents. (i.e., Fixed, Rayleigh, or Uniform (Uniform in Circle). Note: Only available when CORR:ENR:MOD is set to SPOT. See also [:SENSe]:CORRection:ENR:MODe, [:SENSe]:CORRection:ENR:SPOT:ENR, [:SENSe]:CORRection:ENR:UNCertainty, [:SENSe]:CORRection:ENR:ONGamma, [:SENSe]:CORRection:ENR:OFFGamma, [:SENSe]:CORRection:ENR:COVerage, [:SENSe]:CORRection:ENR:SPECify, and [:SENSe]:CORRection:TCOLd. |
|
Relevant Modes |
|
Parameters |
|
<character> |
ENR Spot mode's distribution value. Choose from: RAYL - The probability density function (pdf) of the magnitude of the reflection coefficient is a Rayleigh distribution. This is normally the case for specified values when the overall mismatch is due to several interacting impedance transitions within the device. UNIF - A distribution that was historically used in the industry, before the Rayleigh research, as documented in Keysight Application Note 1449-3, but is rarely accurate. Refer to https://literature.cdn.keysight.com/litweb/pdf/5988-9215EN.pdf. FIX - The reflection coefficient magnitude is always at the given level. This is often the case when measured values are used. |
Examples |
CORR:ENR:DIST FIX CORR:ENR:DIST RAYL |
Query Syntax |
CORRection:ENR:DIST? |
Return Type |
Character |
Default |
FIX |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |