[:SENSe]:IQSTream:DHOSt <string>

(Read-Write) Set and query the destination host to send UDP network packets. E.g., “192.168.1.1".

See also, IQST:DPOR, IQST:SRAT, IQST:STARt, IQST:STOP, IQST:PROT,  IQST:SPP, IQST:VITA:MRES, IQST:VITA:MRIP, IQST:VITA:SID,and MEAS:IQAN.

Relevant Modes

IQA (Option 351), Mixed Analyzers (Option 233)

Parameters

 

<string>

Enter an IP address for the destination port for the IQ streaming data packets.

Examples

IQST:DHOS "192.168.1.1" 'Defines the destination host IP to send UDP network packets

Query Syntax

IQST:DHOS?

Return Type

string

Default

"localhost"

Last Modified:

05apr2021

New command (A.12.3x)